Firmware that worked and now it works no more

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware that worked and now it works no more

1,580件の閲覧回数
jag
Contributor IV
Hi, I'm using a 56F8037, Codewarrior 8.2.3 and Quickstart 2.3. I've this firmware (written by me) that was working until last summer (last time I checked). Yesterday I did some modification and is orking no more (even the unmodified version). The only thing that is changed is CW that now is v. 8.2.3 and before was version 8.2 (or even older, maybe 8.1). The debugging tell me nothing. I download the firmware from CW, I enter the debug mode and go step by step to see what happens. When I arrive to the ArchEnableInt() instruction (asm(bfclr #0x0300,SR)) the window goes blank as if the program is running. If I stop the program, it stops _always_ on the same code line: in startup.c where the pll_lock label is (line 300). I've other projects using CW 8.2.3 that works without problem, but this one probably is the only one that I created with an older version of CW and reopened with the 8.2.3. I read the changelog of CW, but I found nothing useful. Some ideas? Thanks Bye Jack
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

668件の閲覧回数
jag
Contributor IV
Ok, false alarm. the vectors.c file was corrupted and with him the interrupt vector. Reverted from an older revision and now the program is working well :smileyhappy: Thanks SVN :smileywink:
0 件の賞賛
返信