Failed to write in RAM..

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to write in RAM..

651 次查看
hrishikesh23
Contributor I

Dear All,

 

                 Can anybody guess what could be the Issue ..under hardware daignostic ..when i carrry out test for reading it continouslyy reads the same value but hte value i write keep on changing..anybody can guess whats going wrong.

 

All configuration files are correct checked with freescale People.

 

Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:22 2011
:  --------------------

 ============================================

  Wrote  0x67 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:29 2011
:  --------------------

 ============================================

  Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:57 2011
:  --------------------

 ============================================

  Read  0x00 at address: 0x00100000
Timestamp:  Tue Dec 20 16:42:59 2011
:  --------------------

标签 (1)
0 项奖励
回复
1 回复

535 次查看
hrishikesh23
Contributor I

Dear All,

 

               Please go through the Attached File.

0 项奖励
回复