FCS, Failure to step

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FCS, Failure to step

1,274件の閲覧回数
Matt1of3
Contributor II

Hi All

 

I have 2 questions

 

1)      The PEmicro drop down menu on the tool bar is turned off, how do I turn it on?

 

2)      I’m having difficulty with the Full Chip Simulator when using the BCLR instruction.  If I try to set a bit in RAM (first page) it will not work, I get a “Target request failed: Failed to step" error.  I also have problems with the Assembler at the same instruction:

 

BCLR  1,$71  will assemble but will not step

BCLR  1,0x71 will not assemble, I get and “End of line expected “ error A2400

BCLR  1,113            will assemble but will not step.

 

When I’m using the BDM the code will run although I get a warning on the BCLR Instructions.  If it Assembles the disassembly looks good to me.

 

Is there a way I can get the simulator to accept bit instructions to low RAM?

 

Thanks and regards,

ラベル(1)
0 件の賞賛
返信
1 返信

1,117件の閲覧回数
Matt1of3
Contributor II

I forgot to include:  CodeWarrior 10,0  MCS08AC16 controller

0 件の賞賛
返信