ELF is not in expected HALT mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ELF is not in expected HALT mode

5,886 Views
sai
Contributor I
When I try to step into next instruction or  somtimes put a break point or do a hard reset from the CodeWarrior IDE I get a message that says:

ELF is not in expected HALT mode or
ELF is not in expected STOP mode

Any idea what this means. Thanks for any inputs.

I'm using USB TAP to connect to target, with a default clock speed of 4.03 MHz. CodeWarrior version 8.7.

-Sai



Message Edited by sai on 2007-08-27 08:13 PM

Message Edited by sai on 2007-08-27 08:15 PM
Labels (1)
0 Kudos
Reply
4 Replies

1,436 Views
scancath
Contributor I
Hi,
 
I'm trying to connect USB TAP to our custom board. I'm getting the following messages
" Failed to freeze at negation of hreset" and "ELF is not in expected HALT mode" messages.

I presume some thing fundamental is wrong with this board. Any pointers on when I would see this type of messages?

Thanks  a bunch,
Prasad 
0 Kudos
Reply

1,436 Views
CrasyCat
Specialist III
Hello
 
I would recommend you to create a new post for that issue.
 
Make sure you specify which target and version of CodeWarrior you are using.
To retrieve that info:
- Start CodeWarrior
- Select Help -> About Freescale CodeWarrior
- Click on "Install Products"
- CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 Kudos
Reply

1,436 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
Can you please give us the tool version used ?
To do that you must:
* CW:
Start the IDE and click on Help | About Metrowerks CodeWarrior.
Click on Installed Products 
Provide us all info displayed.
Or you can save them in a txt file.
Pascal
0 Kudos
Reply

1,436 Views
sai
Contributor I
Another freescaler has posted a reply to this question in CodeWarrior for ColdFire and Power forum.

Thanks anyway.
-Sai
0 Kudos
Reply