Does Codewarrier perform all that is needed to run P&E Multilink ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does Codewarrier perform all that is needed to run P&E Multilink ?

跳至解决方案
1,210 次查看
klem
Contributor II

I am considering  purchase of a P&E multilink (USB-ML-12) for use with Freescale Codewarrier for HS08 devices.

The P&E order form list several associated software packages such as Flash programmer, debugger, programmer,

editor etc. It seems the Codewarrier performs all these functions using the Multilink, true ???

Thanks for any advice

 

Bob

标签 (1)
0 项奖励
回复
1 解答
953 次查看
klem
Contributor II

Jun Zhang:

Thanks for the reply on CodeWarrier/P&E MultiLink along with the link.

I wondered about P&E charging for the software that Freescale provides

via CodeWarrier. Makes it sound like CW is too good to be true or if there

is a "gottcha" hiding somewhere.

Thanks

Bob Westlund

在原帖中查看解决方案

0 项奖励
回复
2 回复数
953 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

yes you can use CW with p&E multilink cable do all the project work. see below for USB BDM Multilink Cable:

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33&CFID=1007554&CFTOKEN=4326c53a8...

0 项奖励
回复
954 次查看
klem
Contributor II

Jun Zhang:

Thanks for the reply on CodeWarrier/P&E MultiLink along with the link.

I wondered about P&E charging for the software that Freescale provides

via CodeWarrier. Makes it sound like CW is too good to be true or if there

is a "gottcha" hiding somewhere.

Thanks

Bob Westlund

0 项奖励
回复