Debug problem of CW for 56F800/E v7.3 with driver patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug problem of CW for 56F800/E v7.3 with driver patch

2,984件の閲覧回数
Aili
Contributor II
Hi,

I am using CW v7.3 to debug my 56F803 target board. I can download and run the code. I can also "step in". However, it won't stop at the breakpoint. It also can not stop when I use "run to cursor".  But,  it does stop  if I insert the instruction "debug" in the assembly source code,  or  "asm(debug)" in the c source code.

Is it something related to my target board? My original target board does not have JTAG connector, and it took me hard time to solder a JTAG connector.
When I use a different DSC target board 56F8013DEMO, everything works fine.

Any suggestions?

Thanks

Aili
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,209件の閲覧回数
duck
Contributor I
Hi:
 
I have the same problem with the 56F8013 demoboard, do you have any advice?
 
thanks!!
0 件の賞賛
返信

1,209件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
I don't remember problem with the V7.3 debugger.
The new version DSC 8.x is available.
Can I suggest you to try this version ?

You can download the DSC 8.0 on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247

The DSC V8.1.1 is available too.
This is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B

You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.

Hope this will help you.
Pascal

0 件の賞賛
返信

1,209件の閲覧回数
Aili
Contributor II
Hi Pascal,
 
Thank you for your suggestion. We ordered a 32K version of CW 8.0, but the problem is still there. I found it is related to the user code. I used PE to develop a simple program and found everything are OK. Since I am studying someone else codes, which is kind of complicated for me ( I was a fan of TI CCS, and just started to use CW), so far I still don't know which instructions cause problem. I will update it when I figure out the problem.
 
Liping
 
0 件の賞賛
返信

1,209件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi Liping,
 
Thanks for the feedback.
Don't hesitate to contact us.
If you find some other details or if you want we investigate the problem, can I suggest you to  to log your request to the Freescale CRM system.
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
Pascal
0 件の賞賛
返信