DSP56F801 flash_over_jtag and XP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56F801 flash_over_jtag and XP

3,120 Views
cwr_whitehead
Contributor I
I'm trying to use the latest version of the 'flash_over_jtag' application (Epsilon 0.7) to program two daisy chained DSP56F801's. The application ran on PC's using Window 2000. We have now upgraded to XP and the application will no longer work.
 
Whenever I try to run the application, I get the following error:
 
I/O port driver not installed
Installing...
I/O port driver cannot be started
Unable to access to I/O driver
 
Thanks in advance (hopefully).

Message Edited by CrasyCat on 2007-04-13 10:44 AM

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,328 Views
DanielM
Contributor III
Hi,

do you have admin rights on your computer? Is it 32 or 64 bit version of XP (the program was not tested on 64-bit XP at all).

Daniel
0 Kudos
Reply

1,328 Views
cwr_whitehead
Contributor I
Hi Daniel,
 
I've solved the problem. Somehow the zlportio.sys file had been corrupted. I downloaded a new copy and replaced it, now everything works. Obvious really.
 
Thanks for the help.
0 Kudos
Reply