Hello all,
I needed a quick response so I submitted a service request also. Here is the answer I got back. This solution will work for me. Thanks XiangJun Rong
I guess that the pin is /DE rather than /DEZ. Regarding the JTAG signals,they are /RESET,/TRST,TDI,TDO,TMS,TCK,/DE,in the all six signals,/DE signal is an output signals,which only indicate that an debug event has happened when the JTAG is in debug mode,it is not used to transfer data or control something,so for some chip with standard JTAG circuit,the pin is removed from package. If you design your target board,you do not have to connect the /DE pin to 14 pin JTAG connector on board if the chip has /DE pin,in other words,you can connect the /DE or not. If the chip does not has /DE pin,you only float the pin 13 of the JTAG connector,it is okay. Hope it can help you.
BR XiangJun Rong -------