DSC v8.3  (Classic IDE) Project add file warnings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DSC v8.3  (Classic IDE) Project add file warnings

1,037 次查看
txsolarguy
Contributor I

I have started a new project and am adding files.  I am getting an odd warning when I add any header (*.h) file.

 

"At least one file could not be added to the selected target"

 

The file shows up in the project tree, but can not be searched.  If I search for a term in the file, it returns nothing.  However, when I build, it knows the file is there.  I defined the same thing in two seperate header files (ex.  #define TEST_DEF 1) and it was caught by the tool when I built.

 

The access paths for where the files are located are correct.

标签 (1)
0 项奖励
回复
1 回复

668 次查看
txsolarguy
Contributor I

Attempting to do a build, even if it fails, corrects the problem of not being able to search inside the files.

0 项奖励
回复