Com port not getting detected in TWRMPC5125

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Com port not getting detected in TWRMPC5125

1,311件の閲覧回数
Champaka
Contributor III

Hi all,

 

 i am using mpc5125 evaluation kit and code warrior 9.2 evaluation version. when i connect the USB cable for the Serial- to -USB bridge to my pc, the  

HC9S08JMXX CDC (COM 11) communication port will not be displayed in the device manager.

it gets detected as USB-UART in other devices under device manager. should i install any device driver to resolve this? or will this com port gets detected only in the lisenced version ?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

991件の閲覧回数
J2MEJediMaster
Specialist I

It sounds like a driver issue. Normally, CodeWarrior does not block debugging due to a license problem.

 

---Tom

0 件の賞賛
返信

991件の閲覧回数
Champaka
Contributor III

Hi Tom,

 

               i am using windows xp and the com port did not get detected.. i tried in windows 7 platform also.. its the same problem.. could you please send me the link for that driver so that i can install it..

 

I am able to debug and download the program using J-TAG.. now i am trying to load the program to nand flash and i am having this issue.

 

I am not able to do the 5th and 6th step mentioned in the MPC512MQXTTRL pdf...

0 件の賞賛
返信

991件の閲覧回数
J2MEJediMaster
Specialist I

I do not have such a driver. I was just saying that the PC is not recognizing the adapter as having a serial port. Whoever made the adapter should have provided driver software that handles the translation from USB to serial.

 

---Tom

0 件の賞賛
返信

991件の閲覧回数
Champaka
Contributor III

Hi,

 

      i installed Freescale_CDC.inf  device driver . Now the COM port is getting detected..

     Hey  thanks for your help...

0 件の賞賛
返信