Codewarrior 8.0 won't run off of windows XP home`

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior 8.0 won't run off of windows XP home`

1,787 次查看
Klasanov
Contributor I
Hey, ok. I have/had vista (its still on my comp, but just on a different harddrive) that ran Codewarrior fairly buggy-like, so I installed XP in a different HDD and installed Codewarrior on that, but whenever I try to run stuff, it gives me errors like "unable to open .class file animation.class" etc. There's 100 of these so its hard to type out.
 
this is happening on other computers as well, but not all computers that run XP (since I also go to school, I have access to a lot of compies).
 
Is there a way I can fix this? I really do not like the environment Vista has set up and I feel very at home with XP so I really want to be able to run codewarrior off XP, you know?
 
Oh, the codearrior version is like 8.0.
 
Also, I'm sorry if I haven't provided all necessary details.
标签 (1)
0 项奖励
回复
1 回复

690 次查看
CrasyCat
Specialist III
Hello
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
    To retrieve that info:
      - Start CodeWarrior
      - Select Help -> About Freescale CodeWarrior
      - Click on "Install Products"
      - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 项奖励
回复