CodeWarrior for Freescale 65800/E v.8.2.3 & working with CD-ROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior for Freescale 65800/E v.8.2.3 & working with CD-ROM

1,407 次查看
Dekabrist
Contributor I

Hi all,

I read .docx file (doun't related to my CW project ) from compact disk & exract disk, then activate CW and lunch  compiling my project. Compiling frequently abort with request insert compact to CD-ROM (see attachment). This problem was solved only after reload my PC.

Is this IDE error or Windows XP personal problem?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

602 次查看
trytohelp
NXP Employee
NXP Employee

Hello,

 

Difficult to determine the cause of the problem.

I think the installation should be corrupted.

I recommend you to re-install the tool.

 

To avoid problem you must:

 - uninstall it,

 - delete the installation folder,

 - re-install the tool.

 

Regards

Pascal

0 项奖励
回复