CodeWarrior Dev Studio for ColdFire  v5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CodeWarrior Dev Studio for ColdFire  v5.1

跳至解决方案
1,583 次查看
ryanfauth
Contributor I

I need to use CodeWarrior Dev Studio for ColdFire  v5.1 for a legacy project.  Where can I find this?

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
1,281 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Ryan.

all Freescale available CodeWarrior Legacy Downloads are listed here:

CodeWarrior Legacy Downloads|Freescale

However CodeWarrior Dev Studio for ColdFire  v5.1 is a very old version ( released before 2005) and it is no longer available on Freescale web site. I don;t know why you want to use that old CW? what chip do you work with? if you use Coldfire V2-V4 derivatives, please use CW v7.2 or CWv10.6 instead:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

thus if you have any CW related question with CW v7.2 or CWv10.6, Freescale is still easy to provide support.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,282 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Ryan.

all Freescale available CodeWarrior Legacy Downloads are listed here:

CodeWarrior Legacy Downloads|Freescale

However CodeWarrior Dev Studio for ColdFire  v5.1 is a very old version ( released before 2005) and it is no longer available on Freescale web site. I don;t know why you want to use that old CW? what chip do you work with? if you use Coldfire V2-V4 derivatives, please use CW v7.2 or CWv10.6 instead:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

thus if you have any CW related question with CW v7.2 or CWv10.6, Freescale is still easy to provide support.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,281 次查看
ryanfauth
Contributor I

Thanks for your reply,

My goal is to use a newer version of the IDE.  The firmware I am working with was originally built with ver5.1 and I would like to confirm that my build environment is correct by first building the project using the original IDE.

I am using CW ver7.2 now.   Is it possible you could send me a copy of ver5.1 that I could run my  preliminary test with?  ( I understand there is no support for this product)

0 项奖励
回复
1,281 次查看
trytohelp
NXP Employee
NXP Employee

Hi Ryan,

The older versions are not available on Web site.

I need to upload the version on pour transweb system.

For tracking ... I will create a SR for this question.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复