CodeWarrior 5.9.0 intermittently takes forever to connect to Cyclone Max 7.80 via Ethrnet for a Debug session.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 5.9.0 intermittently takes forever to connect to Cyclone Max 7.80 via Ethrnet for a Debug session.

Jump to solution
906 Views
loosePointer
Contributor III

Both my PC and the Cyclone Max are on the 192.168 side of a router.  It works for debugging so I think I have the Gateway, Subnet, and IP setup correctly.  And some times it connects Immediately, compiles, and starts the download to the target,,, But more often than not it can takes over 60 seconds to connect before it starts the download.   Is there a "trick" to get it to connect Immediately all the time???  This minute to connect adds up fast with many change a line and test cycles.  Not to mention how annoying it is. Especially since the compile time is trivial,,, the hold up looks to me like it is the connection. Any one else have this problem,,, anyone know of a fix.

 

Windows7 64 bit

Router D-Link DIR-651

 

Setup "looks" like this

{Corporate intranet}

    ||

[Router]

||         ||

[PC] [Cyclone Max]=[Target]

 

Thanks

Labels (1)
1 Solution
579 Views
loosePointer
Contributor III

PE Micro Support was very Helpfull

Hi James,

Please go to project settings -> Debugger -> Remote Debugging -> Pemicro_TCPIP

connection -> Edit Connection.

In attached window, please make sure that Speed variable is set to 0 (lowest

possible value). The higher this value, the bigger is the prescaler and the

slower your target communication rate will be.

Please let me know if it speeds up the Cyclone MAX performance you are

observing.

Best Regards,

Zahar

P&E

View solution in original post

3 Replies
580 Views
loosePointer
Contributor III

PE Micro Support was very Helpfull

Hi James,

Please go to project settings -> Debugger -> Remote Debugging -> Pemicro_TCPIP

connection -> Edit Connection.

In attached window, please make sure that Speed variable is set to 0 (lowest

possible value). The higher this value, the bigger is the prescaler and the

slower your target communication rate will be.

Please let me know if it speeds up the Cyclone MAX performance you are

observing.

Best Regards,

Zahar

P&E

579 Views
trytohelp
NXP Employee
NXP Employee

Hello James,

to investigate the problem we need to know exactly the tool version you're using.

To do that you must:

  Under CodeWarrior IDE (classic)

      Start the IDE and click on Help | About Freescale CodeWarrior.

      Click on Installed Products 

      Provide us all info displayed.

      Or you can save them in a txt file.

The Cyclone interface is manufactured by P&E.

What is the revision of this interface ?

      We could contact P&E to have their feedback too.

Regards

Pascal

579 Views
loosePointer
Contributor III

Thanks for the Reply Pascal,

This is the contents of my Installed Plugins

Installed Products:
CodeWarrior Development Studio for ColdFire Architectures Version 7.1, Build 14
CodeWarrior Development Studio for ColdFire Architectures Version 7.1.2 Patch, Build 11

IDE Version: 5.9.0 Build 3024
Plugins: 107

================================================================================================
ASINTPPC.dll              5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:47 AM         628K     
================================================================================================

================================================================================================
CmdIDE.exe                5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:16 AM         41K      
================================================================================================

================================================================================================
IDE.exe                   5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:09 AM         10.22M   
================================================================================================

================================================================================================
IDENewDialog.dll          5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:47 AM         201K     
================================================================================================

================================================================================================
IDE_MFC60cw.dll           6.00.8665.0               6.0.8665.0                6.0.4.0                   7/9/2008, 5:38 AM         1.59M    
================================================================================================

================================================================================================
IDE_MSL_DLL90_x86.dll     5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:32 AM         296K     
================================================================================================

================================================================================================
InstallHelperKeys.exe     No Version Info           0.0.0.0                   0.0.0.0                   3/22/2005, 11:01 AM       76K      
================================================================================================

================================================================================================
lmgr8c.dll                No Version Info           0.0.0.0                   0.0.0.0                   5/2/2005, 11:09 AM        832K     
================================================================================================

================================================================================================
MWCore5_0.dll             5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:39 AM         236K     
================================================================================================

================================================================================================
MWRADUtils.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:47 AM         260K     
================================================================================================

================================================================================================
Mwregsvr.exe              5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:52 AM         36K      
================================================================================================

================================================================================================
MWRegSvrWinApp.exe        5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:52 AM         36K      
================================================================================================

================================================================================================
PluginLib.dll             5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:33 AM         120K     
================================================================================================

================================================================================================
PluginLib2.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:33 AM         120K     
================================================================================================

================================================================================================
PluginLib3.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:33 AM         120K     
================================================================================================

================================================================================================
PluginLib4.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:34 AM         84K      
================================================================================================

================================================================================================
PluginLib5.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:34 AM         84K      
================================================================================================

================================================================================================
PluginLib6.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:35 AM         84K      
================================================================================================

================================================================================================
SHW32.DLL                                           4.0.1.0                   4.0.1.0                   2/10/2000, 5:15 PM        110K     
================================================================================================

================================================================================================
tcl84t.dll                8.4.12                    8.4.2.12                  8.4.2.12                  9/25/2006, 2:22 PM        576K     
================================================================================================

================================================================================================
utf8conversion.dll        No Version Info           0.0.0.0                   0.0.0.0                   2/15/2008, 12:47 PM       524K     
================================================================================================

================================================================================================
xerces-2_2_0.dll          2, 2, 0                   2.2.0.0                   2.2.0.0                   7/9/2008, 5:51 AM         2.14M    
================================================================================================

================================================================================================
Bin\Plugins\COM
================================================================================================
DebugRegisterMgr.dll      5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:29 AM         116K     
LogPoint.dll              5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:22 AM         56K      
FlashProgrammer.dll       5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:26 AM         5.60M    
HardwareDiagnostics.dll   5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:27 AM         2.09M    
LoadSaveFill_CF.dll       5.8.0.0                   5.8.0.0                   5.8.0.0                   7/11/2008, 5:35 AM        174K     
MakefileExporter.dll      5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:14 AM         256K     
MWActivate.dll            5.9.0.3024                5.9.0.3024                5.9.0.3024                7/9/2008, 6:17 AM         600K     
ObjectInspector.dll       5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:13 AM         332K     
PackAndGo.dll             1,0,0,0110                1.0.0.72                  1.0.0.72                  7/11/2008, 5:39 AM        344K     
PausePoint.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:22 AM         100K     
pe_init.exe               No Version Info           0.0.0.0                   0.0.0.0                   5/5/2009, 12:13 PM        92K      
PE_Plugin.dll             4.27.0.5077               4.27.0.5077               4.27.0.5077               5/5/2009, 9:03 AM         7.42M    
SaveRestoreRegisters.dll  5.7.0.0                   5.7.0.0                   5.7.0.0                   7/11/2008, 5:36 AM        180K     
ScriptPoint.dll           5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:23 AM         124K     
SkipPoint.dll             5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:23 AM         52K      
SoundPoint.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:23 AM         56K      
TipOfTheDay.dll           1,0,0,0110                1.0.0.72                  1.0.0.72                  7/11/2008, 5:39 AM        64K      
DebugDatabase.dll         5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:29 AM         296K     
VariableFormatter.dll     5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:24 AM         52K      
CPPCodeCompletion.dll     5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:16 AM         808K     
CommandWindow.dll         5.9.0.3024                5.9.0.3024                5.9.0.3024                7/9/2008, 6:21 AM         1.01M    
ColdFireWizard.dll        5.2.0110                  5.2.0.72                  5.2.0.72                  7/11/2008, 5:39 AM        928K     

================================================================================================
Bin\Plugins
================================================================================================

================================================================================================
Bin\Plugins\Compiler
================================================================================================
MCFCCompiler.dll          7.0 build 37              5.3.0.37                  5.3.0.37                  11/20/2008, 12:47 AM      2.57M    
PCLintCompiler.dll        1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         80K      
asm_mcf_elf.dll           7.0 build 37              5.0.0.37                  5.0.0.37                  11/20/2008, 12:50 AM      290K     
ELFImporter.dll           1.0 Build 0005            1.0.0.5                   1.0.0.5                   11/20/2008, 12:50 AM      39K      

================================================================================================
Bin\Plugins\Debugger
================================================================================================
CFDebugger.DLL            7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:34 AM        786K     
DisassemblerCF.dll        7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:32 AM        84K      
Dwarf2Symbolics_2_5.DLL   5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:19 AM         280K     
DwarfSymbolics.DLL        5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:18 AM         240K     
StabSymbolics.DLL         5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:18 AM         156K     

================================================================================================
Bin\Plugins\Debugger\protocols
================================================================================================
CFAbatronProtocol.dll     7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:34 AM        199K     
CFCCSProtocol.dll         7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:35 AM        297K     
CFGDIProtocol.dll         7.0.0.111                 7.0.0.111                 7.0.0.111                 4/29/2009, 11:17 AM       135K     
PEMicroProtocol.dll       7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:34 AM        148K     

================================================================================================
Bin\Plugins\Linker
================================================================================================
BatchRunnerPostLinker.dll 2.0.0 Build 8             2.0.0.8                   2.0.0.8                   7/11/2008, 8:44 AM        44K      
BatchRunnerPreLinker.DLL  1.0.0 Build 6             1.0.0.6                   1.0.0.6                   7/11/2008, 8:44 AM        45K      
ExternalBuildLinker.dll   5.9.0.3024                5.9.0.3024                5.9.0.3024                7/9/2008, 6:41 AM         80K      
MCFLinker.dll             7.0 build 37              5.1.0.37                  5.1.0.37                  11/20/2008, 12:47 AM      348K     
PCLintLinker.dll          1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         84K      

================================================================================================
Bin\Plugins\Preference_Panel
================================================================================================
GDIRconn.dll              7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        54K      
PAssemblerCF.dll          5, 0, 0, 1                5.0.0.1                   5.0.0.1                   11/20/2008, 12:50 AM      198K     
PBackEndCF.dll            7.0 build 37              5.3.0.37                  5.3.0.37                  11/20/2008, 12:50 AM      77K      
PBatchRunnerPostLinker.dll 2.0.0 Build 6             2.0.0.6                   2.0.0.6                   7/11/2008, 8:44 AM        45K      
PBatchRunnerPreLinker.dll 1.0.0 Build 5             1.0.0.5                   1.0.0.5                   7/11/2008, 8:44 AM        30K      
PCFGlobalOptimizer.dll    5.3.0.37                  3.0.3.37                  3.0.3.37                  11/20/2008, 12:50 AM      33K      
PCFTarget.dll             7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:37 AM        84K      
PCLintOptions.dll         1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         41K      
PCLintSettings.dll        1.5                       1.5.0.5                   1.5.0.5                   9/4/2003, 4:58 PM         82K      
PDebugCFExcept.dll        7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:37 AM        33K      
PDebugCFInterrupt.dll     7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:37 AM        9K       
PDebugCFReset.dll         7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:37 AM        52K      
PDebuggerPICSettings.dll  1.2.3.777                 1.2.3.777                 1.2.3.777                 7/11/2008, 5:37 AM        50K      
PDebugx86Except.dll       5.9 Build 3024            5.8.0.0                   5.8.0.0                   7/9/2008, 6:43 AM         64K      
PDisassemblerELF.dll      1.2.0 Build 3             1.2.0.3                   1.2.0.3                   11/20/2008, 12:50 AM      45K      
PExternalBuild.dll        1.0.1.0                   1.0.1.0                   1.0.1.0                   7/9/2008, 6:41 AM         64K      
PFrontEndC.dll            5.3 37                    5.3.0.37                  5.3.0.37                  11/20/2008, 12:51 AM      68K      
PLinkerCF.dll             7.0 build 37              5.1.0.37                  5.1.0.37                  11/20/2008, 12:50 AM      49K      
pMWCVS.dll                No Version Info           0.0.0.0                   0.0.0.0                   10/30/2003, 10:08 AM      64K      
pmwSourceSafe.dll         5.5.1.40704               5.5.1.40704               5.5.1.40704               4/8/2004, 1:37 PM         29K      
PnESerialCycMaxRconn.dll  7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        50K      
PnETCPIPCycMaxRconn.dll   7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        49K      
PnEUSBCycMaxRconn.dll     7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        27K      
PnEUSBRconn.dll           7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        27K      
PPreprocessorC.dll        5.3 37                    5.3.0.37                  5.3.0.37                  11/20/2008, 12:51 AM      72K      
PProjectCF.dll            7.0 build 37              5.1.0.37                  5.1.0.37                  11/20/2008, 12:50 AM      30K      
PRConnCCS.dll             1.0.0.2 b002              1.0.0.2                   1.0.0.2                   7/11/2008, 5:37 AM        84K      
PRConnEthernetTapBDM.dll  7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:37 AM        53K      
PRConnPELightning.dll     7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        27K      
PRConnPnE.dll             7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        27K      
PRConnTCP.dll             5.9 Build 3024            5.8.0.0                   5.8.0.0                   7/9/2008, 6:28 AM         36K      
PRConnUSBTapBDM.dll       7.0.0.110                 7.0.0.110                 7.0.0.110                 7/11/2008, 5:36 AM        54K      
PSerialComm.dll           5.9 Engineering Build     5.8.0.0                   5.8.0.0                   7/11/2008, 5:36 AM        29K      
PSourceFolderMapping.dll  5.9 Engineering Build     5.8.0.0                   5.8.0.0                   7/11/2008, 5:37 AM        52K      
PTcpIpComm.dll            5.9 Engineering Build     5.8.0.0                   5.8.0.0                   7/11/2008, 5:36 AM        22K      
PWarningC.dll             5.3 37                    5.3.0.37                  5.3.0.37                  11/20/2008, 12:51 AM      68K      

================================================================================================
Bin\Plugins\Support\ColdFire\Abatron
================================================================================================
bdiifc32.dll              V1.44                     1.0.4.4                   1.0.4.4                   8/16/2007, 7:47 AM        116K     

================================================================================================
Bin\Plugins\Support\ColdFire
================================================================================================

================================================================================================
Bin\Plugins\Support
================================================================================================
CPlusSourceGen.dll        5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:12 AM         272K     
MWComBase.dll             5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:44 AM         64K      
MWComHelpers.DLL          5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:40 AM         460K     
MWRadModel.dll            5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:47 AM         572K     
ObjectWireWizard.dll      5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:37 AM         136K     

================================================================================================
Bin\Plugins\Support\ColdFire\OSBDM
================================================================================================
osbdm-jm60_gdi_cfv234.dll 1, 0, 12, 1               1.0.12.1                  1.0.12.1                  7/6/2009, 4:05 PM         51K      

================================================================================================
Bin\Plugins\Support\ColdFire\pemicro
================================================================================================
unit_cfz.dll              3.25.0.0                  3.25.0.0                  3.25.0.0                  7/23/2007, 6:23 PM        1.55M    

================================================================================================
Bin\Plugins\Support\Common\Comm_IO
================================================================================================
PP_TargetAccess.dll       5.8.0.3024                5.8.0.3024                5.8.0.3024                7/9/2008, 6:25 AM         60K      

================================================================================================
Bin\Plugins\Support\Common
================================================================================================

================================================================================================
Bin\Plugins\Support\Flash_Programmer\File_IO
================================================================================================
BIN_File_IOEngine.dll     5.8.0.3024                5.8.0.3024                5.8.0.3024                7/9/2008, 6:25 AM         26K      
ELF_File_IOEngine.dll     5.8.0.3024                5.8.0.3024                5.8.0.3024                7/9/2008, 6:25 AM         21K      
SREC_File_IOEngine.dll    5.8.0.3024                5.8.0.3024                5.8.0.3024                7/9/2008, 6:25 AM         35K      

================================================================================================
Bin\Plugins\Support\Flash_Programmer
================================================================================================

================================================================================================
Bin\Plugins\Support\Sim\ccssim2\bin
================================================================================================
ccssim.dll                No Version Info           0.0.0.0                   0.0.0.0                   12/1/2005, 11:11 PM       815K     
ccssim2.exe               No Version Info           0.0.1.1                   0.0.1.1                   10/20/2004, 4:24 AM       153K     
elfioloader.dll           No Version Info           0.0.0.0                   0.0.0.0                   10/20/2004, 4:24 AM       227K     
libcf2e.dll               No Version Info           0.0.0.0                   0.0.0.0                   10/20/2004, 4:24 AM       228K     
libcf2iss.dll             No Version Info           0.0.0.0                   0.0.0.0                   3/22/2006, 3:41 PM        184K     
libcf4e.dll               No Version Info           0.0.0.0                   0.0.0.0                   10/20/2004, 4:24 AM       232K     
libcf4iss.dll             No Version Info           0.0.0.0                   0.0.0.0                   10/6/2005, 6:07 PM        488K     
lmgr8c.dll                No Version Info           0.0.0.0                   0.0.0.0                   11/17/2004, 5:45 PM       832K     
tcl82.dll                 8.2.3                     8.2.2.3                   8.2.2.3                   10/20/2004, 4:24 AM       456K     
tk82.dll                  8.2.3                     8.2.2.3                   8.2.2.3                   10/20/2004, 4:24 AM       817K     
winico03.dll              No Version Info           0.0.0.0                   0.0.0.0                   10/20/2004, 4:24 AM       77K      

================================================================================================
Bin\Plugins\Support\Sim\ccssim2
================================================================================================

================================================================================================
Bin\Plugins\Support\Sim
================================================================================================

================================================================================================
Bin\Plugins\version_control
================================================================================================
mwcvs.dll                 No Version Info           0.0.0.0                   0.0.0.0                   10/30/2003, 10:08 AM      232K     
mwSourceSafe.dll          1.0.3.716                 1.0.3.716                 1.0.3.716                 4/8/2004, 1:37 PM         137K     
VCSClearCase.dll          1.1.2.1999                1.1.2.1999                1.1.2.1999                8/16/2004, 1:18 PM        76K      

================================================================================================
Bin\resource
================================================================================================
CPlusResources.dll        5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:10 AM         24K      
ExternalBuildResources.dll 5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:41 AM         6K       
IDEAuxiliaryResources.dll 5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:40 AM         44K      
IDEResources.dll          5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 5:40 AM         52K      
MakefileResources.dll     5.9.0 Build 3024          5.9.0.3024                5.9.0.3024                7/9/2008, 6:10 AM         12K      

0 Kudos