Changing variables stored in flash from the freemaster's project.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Changing variables stored in flash from the freemaster's project.

2,328 次查看
Phantom_
Contributor I

How ? :smileyhappy:

DSP56805

FreeMaster 1.38

I read more doc's but cant program flash from FreeMaster.

I need change constant variables on flash only.

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

906 次查看
Phantom_
Contributor I

Problem solved.

topic closed.

0 项奖励
回复

906 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

Do you want to have information reggarding Freesmaster ?

Like how to show variable in this tool ?

 

Regards

Pascal

0 项奖励
回复

906 次查看
Phantom_
Contributor I

not show.

in the Freemasters docs i find information about ActiveX "SendCommand".

I wont write function in 56F805 programm, that stored variables from memory to flash,  and start this function via FreeMaster's "SendCommand".

Can i do that ?

0 项奖励
回复