Changing variables stored in flash from the freemaster's project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing variables stored in flash from the freemaster's project.

2,381件の閲覧回数
Phantom_
Contributor I

How ? :smileyhappy:

DSP56805

FreeMaster 1.38

I read more doc's but cant program flash from FreeMaster.

I need change constant variables on flash only.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

959件の閲覧回数
Phantom_
Contributor I

Problem solved.

topic closed.

0 件の賞賛
返信

959件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

 

Do you want to have information reggarding Freesmaster ?

Like how to show variable in this tool ?

 

Regards

Pascal

0 件の賞賛
返信

959件の閲覧回数
Phantom_
Contributor I

not show.

in the Freemasters docs i find information about ActiveX "SendCommand".

I wont write function in 56F805 programm, that stored variables from memory to flash,  and start this function via FreeMaster's "SendCommand".

Can i do that ?

0 件の賞賛
返信