CW10 debug problem with windows VISTA, not in W-XP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW10 debug problem with windows VISTA, not in W-XP

1,221 次查看
cocheca
Contributor I

Hi,

I have two problem in windows VISTA with CW10.

 

1.- When CW10 starts  this message appear in the console:

"...

ORB could not be initialized. Aborting connection.

java.net.ConnectException: Connection timed out: connect.

 

Anyone knows this problem ?

 

2.- When I try to debug a project, in 87% of the process, appear a windows error. It says:

"Could not set PC to entry point"

 

These problems don't happen in W-XP. I test the CW10 with the same project and same configuration.

Would appreciate any help.

Thanks. Regards Jose

标签 (1)
0 项奖励
回复
1 回复

767 次查看
cocheca
Contributor I

Sorry, I forgot to mention my target.

 

It's TWR-51CN

s/n 309301203.

SCH-26003 REV E

700-26003 REV B

 

The OSBDM firmware was upgraded to the version comming in the CW10 directory.

 

Thanks in advance.

 

Jose.-

0 项奖励
回复