CW can't find ARTDIVREC_S16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW can't find ARTDIVREC_S16

跳至解决方案
2,780 次查看
GaryOlmstead
Senior Contributor I

I am using the 56F8323 and CW v5.6.1 to write a program that includes floating point calculations.  It compiles OK, but I am getting a link error that says that ARTDIVREC_S16 is undefined. 

 

I tried adding all the 56800E float libraries I could find, all to no avail.  I found a sample application that uses fp and ARTDIVREC_S16.  It is demo_v42bis.mcp, and it includes only FP56800.lib, and MSL C 56800.lib. 

 

I already had MSL C 56800E.lib (along with fplib_advan_smm.lib, fllib_balan_smm.lib, plib_fast_smm.lib, and MSL C 56800E smm.lib).  I couldn't find anything called FP56800E.lib, and when I tried adding FP56800.lib, I got an error saying that it's for a different processor.

 

So, where is ARTDIVREC_S16 for the 56800E, or is there another way to make the error go away?  I tried searching for the ARTDIVREC_S16 source code, but couldn't find that, either.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,697 次查看
GaryOlmstead
Senior Contributor I

Hi Pascal --

 

"I don't understand why you get this error.

Please can you provide us your project showing the problem`?"

 

I don't understand it either, but when I added the file manually, the error went away.  I had the same problem with an add and a multiply, but adding ftlib_fast_smm.lib fixed both of those.  My question is why related code is not co-located, but that isn't your responsibility, so I'll let it go.

 

Thanks for your help.

 

Gary

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,697 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

 

The CodeWarrior for DSC contains 2 development tools for DSP and DSPE.

Your project refers to DSP56F8323. It's a DSPE.

The lib FP56800.lib is for DSP and not for DSPE.

ARTDIVREC_S16 is a runtime function.

By default it's called by the compiler code generated.

This function is included in the ARTDIVREC_S32_01.asm file located in the folder:

  CodeWarrior for DSC56800E v8.2.3\M56800E Support\runtime_56800E\rtmpy_upperresult

 

I don't understand why you get this error.

Please can you provide us your project showing the problem`?

 

Regards

Pascal

0 项奖励
回复
1,698 次查看
GaryOlmstead
Senior Contributor I

Hi Pascal --

 

"I don't understand why you get this error.

Please can you provide us your project showing the problem`?"

 

I don't understand it either, but when I added the file manually, the error went away.  I had the same problem with an add and a multiply, but adding ftlib_fast_smm.lib fixed both of those.  My question is why related code is not co-located, but that isn't your responsibility, so I'll let it go.

 

Thanks for your help.

 

Gary

 

0 项奖励
回复