CW_68K_V3.2.exe (codewarrior for the 68K)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW_68K_V3.2.exe (codewarrior for the 68K)

2,061 Views
stefanorocca
Contributor II
Hello to All,
 
I purchased  CWA-PRO-FL instead of a CWA-PRO-NL: my PC is not a server.
While I'm waiting for a solution from the support, I need to start to work on it immediately.
 
For solving this situation (and while the support replis me), I downloaded the trial version (valid for 30 days) of the codewarrior for the M68K.
 
Despite the information, no license is contained: the license.dat file is empty and the program doesn't run.
Can someone help me?
 
Stefano 
Labels (1)
0 Kudos
Reply
2 Replies

585 Views
stefanorocca
Contributor II
Problem solved.
 
The Customer Support changes my license to a node locked (NL) version.
 
Stefano
0 Kudos
Reply

585 Views
J2MEJediMaster
Specialist I
Glad to hear you got the licensing issue solved. And you did the right thing, which is worth pointing out here.

We've got an automated system that doles out CodeWarrior licenses. As developers, you know that occasionally such a complex system can misfire. When that happens, in order get you a working license as fast as possible--as well as bring the error condition to our attention so that the automated system can be improved--it's best to file a Service Request (SR) on any licensing problem.

---Tom
0 Kudos
Reply