CW 10.1 can not close and does not remember last workspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.1 can not close and does not remember last workspace

799件の閲覧回数
barbercolman
Contributor III

HI

Each time I start CW 10.1 I have change to the correct workspace even If I have the use as default checked. Any idea what is wrong? Also Windows sometines complains the CW does not exit.

ラベル(1)
0 件の賞賛
返信
1 返信

658件の閲覧回数
CrasyCat
Specialist III

Hello

 

Are you using the tools on a Windows 7 host?

If this is the case can you try to uninstall CodeWarrior and install it outside of the Program Files  folder.

For instance using C:\Freescale as root instead of C:\Program Files (x86)\Freescale.

 

It looks like you do not have write access to the CodeWarrior installation directory. 

 

CrasyCat

0 件の賞賛
返信