CW 10.1 can not close and does not remember last workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.1 can not close and does not remember last workspace

796 Views
barbercolman
Contributor III

HI

Each time I start CW 10.1 I have change to the correct workspace even If I have the use as default checked. Any idea what is wrong? Also Windows sometines complains the CW does not exit.

Labels (1)
0 Kudos
Reply
1 Reply

655 Views
CrasyCat
Specialist III

Hello

 

Are you using the tools on a Windows 7 host?

If this is the case can you try to uninstall CodeWarrior and install it outside of the Program Files  folder.

For instance using C:\Freescale as root instead of C:\Program Files (x86)\Freescale.

 

It looks like you do not have write access to the CodeWarrior installation directory. 

 

CrasyCat

0 Kudos
Reply