As in topic, can i write commercial appliciation with CW 10.1 special suite ? In license agreement i've found only this.
" Evaluation Period The Software may allow you to install it on a machine without paying a license fee. The Software will operate until a certain time elapses (“Evaluation Period”) and will then automatically disable itself. Until then, Freescale grants to you the non-transferable right to install the software onto a single computer and to use the Software on that computer. You may not use the Software for commercial purposes during the Evaluation Period."
But as far i understand there is no Evaluation Period on special edition.
Regards, Lukas
解決済! 解決策の投稿を見る。
That is correct. The Special Edition is a limited version of the CodeWarrior tools from the start. There is not an evaluation period. The Evalation Edition allows you to try a fully-featured version of the CodeWarrior tools for 30 days.
---Tom
So i can use CW special Edition for commercial purposes?
If you can work within the code size limit of the Special Edition tools, yes.
---Tom