CW 10.1 Compiler crashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 10.1 Compiler crashing

984 次查看
javier1
Contributor III

When I compile the project, CW 10.1 released the following error...

 

ARM C/C++ Compiler has encountered an error and needs to close

 

make:***(Sources/main.obj)Error -1073741811

 

someone knows that can happen?

 

thanks to all

标签 (1)
0 项奖励
回复
4 回复数

580 次查看
CrasyCat
Specialist III

Hello

 

I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.

CrasyCat

0 项奖励
回复

580 次查看
javier1
Contributor III

ok, i do. Regards 

0 项奖励
回复

580 次查看
buraksoner
Contributor II

Hello!

I have a similar problem, is this solved in any way?

Regards,

Burak

0 项奖励
回复

580 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Burak,

this is a thread that was posted 5 years ago.

Now we always encourage customer to use the latest CW10.6.4

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

please test your problem  with CW10.6.4 with creating a new workspace and new project.

if problem persists, please create a new question for it rather than post the thread under the old one.

thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复