Binary file size is greater even for a simple program in CW v9.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Binary file size is greater even for a simple program in CW v9.2

跳至解决方案
1,541 次查看
Champaka
Contributor III

Hi,

         I have created a simple hello world program in code warrior V9.2.

        Binary file size of this program is 4036 KB. where as in the older version , code warrior V8.5, binary file size of the same program takes only     

        33 KB.

          Could anyone tell me the reason for this. I would also like to know how to reduce the binary file size in code warrior V9.2.

标签 (1)
1 解答
1,233 次查看
stanish
NXP Employee
NXP Employee

Hello,

Could you possibly compare if the .lcf files are the same in both cases (v9.2 vs. v8.5).

I suspect there might be a gap between two sections. The binary file cannot "skip" the gaps then its size may be much bigger in comparison to e.g.  s19 or elf file.

Another option is to enable Linker option "generate multiple binary files". in this case if there is a address gap between two sections a separate binary file for each section is created.

Can you post your .lcf + .map files for both cases (v9.2 vs. v8.5) for further analysis if the suggestion above does not help.

Thanks

Stan

在原帖中查看解决方案

2 回复数
1,234 次查看
stanish
NXP Employee
NXP Employee

Hello,

Could you possibly compare if the .lcf files are the same in both cases (v9.2 vs. v8.5).

I suspect there might be a gap between two sections. The binary file cannot "skip" the gaps then its size may be much bigger in comparison to e.g.  s19 or elf file.

Another option is to enable Linker option "generate multiple binary files". in this case if there is a address gap between two sections a separate binary file for each section is created.

Can you post your .lcf + .map files for both cases (v9.2 vs. v8.5) for further analysis if the suggestion above does not help.

Thanks

Stan

1,233 次查看
Champaka
Contributor III

Thanks for the reply Stan. Same thing was done and it was solved.

0 项奖励
回复