9s08 controller internal EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9s08 controller internal EEPROM

1,842 Views
maddularajesh
Contributor III

Hai , Iam using 9S08DZ60 controller internal EEPROM. while accessing iam getting Access Error.Please kindly suggest the different root causes. I have configured Clock as 200KHZ(PLL Freq is 32MHZ, Selected PRDIV is 1 and DIV factor as 9). Is there any register to be configured for enabling clock. Please kindly share any Software routines available.

Thanks & Regards,

M.N.V.Rajesh

Tags (2)
0 Kudos
Reply
2 Replies

1,582 Views
tonyp
Senior Contributor II

In case it helps, I have the following DZ-specific EEPROM library but it's written in macro assembly language:

EEPROM access library in assembly language for 68HCS08 DZ-compatible MCUs

0 Kudos
Reply

1,582 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I have a  S08DZ eeprom demo project and doc.

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply