This tutorial demonstrates how to convert a Tensorflow model to TensorFlow Lite using post training quantization and run the inference on an i.MX8 board using the eIQ™ ML Software Development Environment. It uses a TensorFlow mobilenet_v1 model pre-trained with ImageNet.
NOTES:
1. Except for the section "Build Custom Application to Run the Inference" this tutorial can also be applied to any i.MX RT platform.
2. For more information on quantization check the 'QuantizationOverview.pdf' attached to this post.
$: bitbake fsl-image-qt5 -c populate_sdk
$: ./$YOCTO_BUILD_FOLDER/bld-wyland/tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-fsl-image-qt5-aarch64-toolchain-4.14-sumo.sh
$: conda create -n tf_env pip python=3.6
$: conda env list
$: conda activate tf_env
$: pip install tensorflow==1.12.0
NOTE: make sure that the installed TensorFlow version is the same as the one used in eIQ (currently 1.12)
$ git clone https://github.com/tensorflow/tensorflow.git
$ cd tensorflow
$ git checkout r1.12
$: mkdir ~/tf_convert
$: cd ~/tf_convert/
$: wget http://download.tensorflow.org/models/mobilenet_v1_2018_08_02/mobilenet_v1_1.0_224.tgz
$: tar -xzvf mobilenet_v1_1.0_224.tgz
NOTE: On the tensorflow github there are multiple model versions available for MobileNet_v1. The intention is to provide different options to fit various latency and size budgets. For this tutorial mobilenet_v1_1.0_224 is used. For a brief explanation of the naming convention:
import tensorflow as tf
graph_def_file = 'mobilenet_v1_1.0_224_frozen.pb'
input_arrays = ["input"]
output_arrays = ["MobilenetV1/Predictions/Reshape_1"]
converter = tf.contrib.lite.TFLiteConverter.from_frozen_graph(graph_def_file, input_arrays, output_arrays)
converter.post_training_quantize = True
tflite_model = converter.convert()
open("converted_model.tflite", "wb").write(tflite_model)
NOTE: for details on how to set the values for 'input_arrays' and 'output_arrays' see section 'How to obtain input_arrays and output_arrays for conversion'
$: conda activate tf_env
$: python convert.py
NOTE: notice that after quantization the model size was reduced ~x4 times in moving from 32-bits to 8-bit.
This tutorial describes two ways to obtain this data: using tensorflow API to inspect the model and dump the information OR using a GUI tool to visualize and inspect the model. Both will be detailed in the following sections.
$: wget https://gist.githubusercontent.com/sunsided/88d24bf44068fe0fe5b88f09a1bee92a/raw/d7143fe5bb19b8d5beb...
$: python dump_operations.py mobilenet_v1_1.0_224_frozen.pb > ops.log
$: vim ops.log
Operations:
- Placeholder "input" (1 outputs)
- Const "MobilenetV1/Conv2d_0/weights" (1 outputs)
- ...........
- Shape "MobilenetV1/Predictions/Shape" (1 outputs)
- Reshape "MobilenetV1/Predictions/Reshape_1"(1 outputs)
Netron is a viewer for neural network, deep learning and machine learning models.
Install it on the Ubuntu host and use it to inspect the *.pb tensorflow frozen model:
$: pip install netron
$: netron mobilenet_v1_1.0_224_frozen.pb
Serving 'mobilenet_v1_1.0_224_frozen.pb' at http://localhost:8080
Open the specified page in the browser to visualize the graph and check the name of the first and last node:
TF_REPO - full path to the tensorflow repo (see Prerequisites section for details)
MOBILENET_PATH - full path to the location of the mobilenet_v1 models (see Prerequisites section for details)
YOCTO_SDK - full path to the location of the YOCTO SDK install folder (see Prerequisites section for details)
BOARD_IP - IP of the i.MX8 board
$: cd $TF_REPO/tensorflow/contrib/lite/examples/label_image/
$: source $YOCTO_SDK/environment-setup-aarch64-poky-linux
$: $CXX --std=c++11 -O3 bitmap_helpers.cc label_image.cc -I $YOCTO_SDK/sysroots/aarch64-poky-linux/usr/include/tensorflow/contrib/lite/tools/make/downloads/flatbuffers/include -ltensorflow-lite -lpthread -ldl -o label_image
$: scp label_image root@$BOARD_IP:~/tflite_test
$: scp $MOBILENET_PATH/converted_model.tflite root@$BOARD_IP:~/tflite_test
$: scp -r testdata root@$BOARD_IP:~/tflite_test
$: scp ../../java/ovic/src/testdata/labels.txt root@$BOARD_IP:~/tflite_test
$: ./label_image -m converted_model.tflite -t 1 -i testdata/grace_hopper.bmp -l labels.txt
Loaded model converted_model.tflite
resolved reporter
invoked
average time: 571.325 ms
0.786024: 653 military uniform
0.0476249: 466 bulletproof vest
0.0457234: 907 Windsor tie
0.0245538: 458 bow tie
0.0194905: 514 cornet
ここにコメントを追加するには、ご登録いただく必要があります。 ご登録済みの場合は、ログインしてください。 ご登録がまだの場合は、ご登録後にログインしてください。