SEGGER AppWizard Enabling Advanced GUI Design with MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEGGER AppWizard Enabling Advanced GUI Design with MCUXpresso

nxf42461
NXP Employee
NXP Employee
2 1 3,130

The purpose of this Blog is to assist new users of the AppWizard to create and run their first project. The AppWizard is a tool for creating complete and ready-to-use emWin applications. The tool makes it very easy to build an application, manage resources and even define the application’s behavior.

 

Managing resources of an application is also made incredibly easy since the user simply has to add their resources to the project. All of the rest is done by the AppWizard, this means the user doesn’t have to fiddle around with dozens of resource files anymore.

 

pastedImage_1.png

 

Installation

You can find the download link for the Tool from the below link.

NXP emWin Libraries | NXP    

To install the AppWizard, simply run the setup wizard which will guide you through the installation. It comes with all required components without having to download nor install further tools.

pastedImage_7.png

Creating a new AppWizard project

1.    Run the SEGGER AppWizard from your desktop.

         pastedImage_9.png

2.   Click Create a new project.

3.   Choose a Project path. Give your AppWizard project a name in the Project name field.
      Select a BSP for this project. Then click Ok.

      pastedImage_10.png

Using the SEGGER AppWizard with NXP MCUXpresso

We have an Application Note Release Coming up which enables to Integration of the AppWizard Project with the MCU Xpresso Project,

To help you start up with the Integration I have created a basic reference project which has around 4 screens and switch whose press will help you switch between all the screens. Attached are the projects (MCUXpresso and Appwizard) for your further reference.

1 Comment
nxf33441
NXP Employee
NXP Employee

For more information on getting started with emWin, AppWizard and MCUXpresso, check out MCU Tech Minutes | GUI Development With emWin and AppWizard.