setenv hwconfig 'fsl_ddr:bank_intlv=auto;core_prefetch:disable=0xFE'
qixis reset altbank (reset the board - in case using bank 0 run 'qixis reset' only)
Make sure you see the same in ‘cat /proc/cmdline’ once kernel is booted:
- use 1G hugepages:
default_hugepagesz=1024m hugepagesz=1024m hugepages=6 (or any number)
- isolate cpu's for user space (for the CPUs running DPDK without kernel interference):
isolcpus=1-7
- make sure no rcu stalls and watchdog prints:
nmi_watchdog=0 rcupdate.rcu_cpu_stall_suppress=1
source /usr/local/dpdk/enable_performance_script.sh
(please make sure that you are not using core 0 in the DPDK coremask/lcores - i.e. the core, which is also running the Linux OS services)
cat /proc/interrupts (search for dpio interrupts and their corresponding irq numbers)
cat 0x1 > /proc/irq/<irq number>/smp_affinity (for enabling Core 0 to serve interrupts on DPIO)
Run above command for all the dpio portals
e.g. For running testpmd in multiqueue mode:
on running testpmd use CLI option '--rxq=<x>' to create ‘x’ rx queues.
For 2 queues use --rxq=2 parameter. For e.g.
./testpmd -c 0x3 -n 1 -- -i --nb-cores=1 --portmask=0x10 --port-topology=chained --rxq=2
Note 1: default l2fwd example application does not support multiqueues with packet distribution.
Note 2: In case of multiple queues, use adequate number of flows per port (e.g 1K flows per port) so flows can evenly distribute across cores.
只有注册用户才能在此添加评论。 如果您已经注册,请登录。 如果您还没有注册,请注册并登录。