NXP PSIRT was informed by security researchers about two Denial of Service (DoS) vulnerabilities which can cause crashes or message-dependent deadlocks in certain Bluetooth Low Energy (Bluetooth LE) implementations of the MCUXpresso Software Development Kit (SDK). The specific software vulnerabilities are:
If the SoC receives a Bluetooth LE Link Layer (LL) packet with a length greater than expected, the packet is not discarded and causes the SoC to crash.
If the SoC receives a Bluetooth LE packet with a Link Layer ID (LLID) = 0, then memory content adjacent to the packet receiving buffer is overwritten, which causes the Bluetooth LE stack to malfunction and enter in deadlock.
Exploiting these software vulnerabilities requires the following conditions to be in place:
NXP has released updated MCUXpresso SDKs with mitigations to address these specific software vulnerabilities and recommends users to update any impacted solutions to the latest respective MCUXpresso SDK versions.
Devices | MCUXpresso SDK Version with the Mitigations |
---|---|
MKW39xxxxxxxx MKW38xxxxxxxx MKW37xxxxxxxx |
|
NOTE: MCUXpresso SDK mitigations for MKW40xxxxx/MKW30xxxxx and K32Wxxxxx devices will be released separately. Other products in our Bluetooth LE portfolio are being analyzed and any future updates will be published on this page.
NOTE: Customers who have previously downloaded the MCUXpresso SDK and have the notification preferences turned on (default), should have automatically received an update on the latest MCUXpresso SDK releases.
Please have the Content update checkbox ticked to allow notifications for future MCUXpresso SDK updates.
The SweynTooth series of vulnerabilities impact many Bluetooth LE stack implementations from other software and device suppliers. NXP strongly encourages users to review all Bluetooth LE stack implementations with their vendors to ensure that they are not impacted by these vulnerabilities.
NXP recommends users review these descriptions for their specific use cases to ascertain any impact to their own products or end customers and take any necessary actions.
NXP PSIRT would also like to thank Matheus E. Garbelini, Sudipta Chattopadhyay, and Chundong Wang of the Singapore University of Technology and Design for their responsible disclosure.
For additional questions or support please contact your local NXP representative or submit a ticket at https://support.nxp.com/
______________________________________________________________________________________________
Please note this information is preliminary and subject to change. To the best of NXP's knowledge, the information contained herein is accurate and reliable as of the date of publication; however, NXP does not assume any liability for the accuracy and completeness of the information.
Information in this document is provided solely to enable system and software implementers to use NXP products. There are no express or implied copyright licenses granted hereunder to design or fabricate any integrated circuits based on the information in this document. NXP reserves the right to make changes without further notice to any products herein. NXP makes no warranty, representation, or guarantee regarding the suitability of its products for any particular purpose, nor does NXP assume any liability arising out of the application or use of any product or circuit, and specifically disclaims any and all liability, including without limitation consequential or incidental damages. “Typical” parameters that may be provided in NXP data sheets and/or specifications can and do vary in different applications, and actual performance may vary over time. All operating parameters, including “typicals,” must be validated for each customer application by customerʼs technical experts. NXP does not convey any license under its patent rights nor the rights of others. NXP sells products pursuant to standard terms and conditions of sale, which can be found at the following address: nxp.com/SalesTermsandConditions.
While NXP has implemented advanced security features, all products may be subject to unidentified vulnerabilities. Customers are responsible for the design and operation of their applications and products to reduce the effect of these vulnerabilities on customer's applications and products, and NXP accepts no liability for any vulnerability that is discovered. Customers should implement appropriate design and operating safeguards to minimize the risks associated with their applications and products.
You must be a registered user to add a comment. If you've already registered, sign in. Otherwise, register and sign in.