Compile the sample project within MCAL, like S32K14X_MCAL4_2_RTM_1_0_0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compile the sample project within MCAL, like S32K14X_MCAL4_2_RTM_1_0_0

Compile the sample project within MCAL, like S32K14X_MCAL4_2_RTM_1_0_0

Hi, 

   If you try to compile the sample project within S32K14X_MCAL4_2_RTM_1_0_0, you should take care of the command if you use Linaro.

   After you set the environment of compiling and run the command under command window, you should enter 

   "launch.bat MODE=USER TOOLCHAIN=linaro"

   NOT

   "launch.bat MODE=USER TOOLCHAIN=LINARO"

 

   The command is case sensitivity.  

Hope you can compile the project successfully. 

Cheers!

Oliver

Tags (3)
No ratings
Version history
Last update:
‎07-30-2020 01:53 AM
Updated by: