Problem:Icu configuration about MCAL4_3

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem:Icu configuration about MCAL4_3

跳至解决方案
6,292 次查看
Ada_Lovelace
Contributor IV

Dear all,

I have a problem, it has an error when I use the demo about  lightning_MPC5777C_4.3_Split.

The demo is based on AUTOSAR\MPC5777C_MCAL4_3_RTM_1_0_0\MPC5777C_MCAL4_3_RTM_1_0_0_Sample_Application.

The problem is about the ICU configuration, I can not choose the 'ICU_MODE_SIGNAL_MEASUREMENT',it tells me that I must enable the IcuSignalMeasurement optional container, but I can not find the way to enable it.

Could anybody can tell me, how to solve the problem?

thanks.

pastedImage_1.png

pastedImage_2.png

标记 (3)
0 项奖励
回复
1 解答
6,205 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

在原帖中查看解决方案

0 项奖励
回复
2 回复数
6,145 次查看
eleanor
Contributor I

Follow this steps

1. Edge detection uses ECNT instruction. Please refer to N2HET instruction set in TRM

2. Signal measurement (duty, Period): use PCNT instruction. Please refer to N2HET instruction set in TRM.

0 项奖励
回复
6,206 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

Hope this helps,

Marius

0 项奖励
回复