Dear all,
I have a prolem, when I use the MCAL4_3 , I configurate the ADC,but It has the error.
When I choose the continuous mode and "without interrupt" mode, it has an error that:without interrupt feature is not supported for continuous conversion mode.
Do MPC5777C must use interrupt mode about continuous mode?
Or there is a problem about MCAL4_3?
解決済! 解決策の投稿を見る。
I have solved the problem.MCAL4_3 version has the bug , update the MCAL4_3 , ADC calibration makes it work.
I have solved the problem.MCAL4_3 version has the bug , update the MCAL4_3 , ADC calibration makes it work.
 
					
				
		
 mariuslucianand
		
			mariuslucianand
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello cuihan.ma@dotrustech.com,
In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745
Hope this helps,
Marius