what's the difference p2p and star-network in software design?  MC13211

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what's the difference p2p and star-network in software design?  MC13211

1,422 次查看
Beijing2008
Contributor I
Dear all:
 
   I plan to use the MC13211 and SMAC codebase,I need your helpness.
   I knew the SMAC support Point-to-Point or star-network applicaiton.
   My question is :
   On the Point-to-Point  and Star-Network, what' s difference them in software design of C code level?
   Whether need a coordinater in star-network?
   I'm puzzled!
 
   Thanks for your suggestion!
 
best regards,
Charly
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-06-30 02:27 PM
标签 (1)
0 项奖励
回复
1 回复

730 次查看
Beijing2008
Contributor I
Now, my understanding is : The star network of Zigbee only include one Server,it is a controller,and other end devices are Client,similar the TCP/IP network.All the clients can connect with the Server at the same time.
 
However, the Point-to-Point network is a especially star network,it also has one Server,but it only allows one Client to connect with itself! Other client will be prohibited. The client number is limited.
 
Is it right? please help me to confirm it!
 
Thanks and best regards!
 
Charly
 
0 项奖励
回复