setting ICG1 in gb60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

setting ICG1 in gb60

1,390件の閲覧回数
snaeth
Contributor I
1
ラベル(1)
0 件の賞賛
返信
1 返信

728件の閲覧回数
peg
Senior Contributor IV
Hi Confused,
 
Need more info here.
Presumably you are driving the GT clock from the radio?
If so what is the frequency, it is a selectable division of the xtal in the radio.
Did you mean 16KHz or MHz?
Are the frequencies you quote, clock or buss?
Approx. 8MHz is the default clock speed out of reset if this gives any clue.
 
P.S. putting the code in a source box give fixed width font which makes the arrows line up.

Message Edited by peg on 2007-03-2909:27 PM

0 件の賞賛
返信