how to work with the rs08 bdc commands in cw 5.1 special edition?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to work with the rs08 bdc commands in cw 5.1 special edition?

1,842 Views
iejiel
Contributor I
 
I bougth PEmicro USB hcs08 multilink rev c and it programs the flash of the rs08 but I can not in circuit debbug because CW 5.1 for hc(s)08 special edition does not recognize any bdc command.
 
I get for instance:
in>background
Error: no such command: background
If the command exists, open the matching component and try it again.

All the other commands (such as go,stop,t,etc.)work well.
 
 
Labels (1)
0 Kudos
Reply
2 Replies

919 Views
CrasyCat
Specialist III
Hello
 
What are you trying to achieve here?
What is bdc command expected to do?
 
CrasyCat
0 Kudos
Reply

919 Views
iejiel
Contributor I
Hello CrasyCat,
 
I use mc9rs08ka2 as taget MCU and I want to debbug it using the active background mode commands (read_ status,write_control,etc.) with pemicro usb multilink and cw5.1.
 
I just now received the following explanation that give me the answer:
BDC command can not run in command window. BDC command is a protocol
just for USB HCS08 Multilink communicating with target MCU.
You can type 'help' in command to get all commands that can running in
command window.
So, the commands that you can run in command window and BDC commands
are
very different system.
Generally, Hiwave will send the command you ran in command window to
Multilink and Multilink will translate this command to BDC command and
then send it to target MCU.
Best Regards,
Yong
Technical Support
Freescale Semiconductor
 
 
Thanks,and excuse me,my english is not good I speak spanish.
 
0 Kudos
Reply