how to work with the rs08 bdc commands in cw 5.1 special edition?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to work with the rs08 bdc commands in cw 5.1 special edition?

1,850件の閲覧回数
iejiel
Contributor I
 
I bougth PEmicro USB hcs08 multilink rev c and it programs the flash of the rs08 but I can not in circuit debbug because CW 5.1 for hc(s)08 special edition does not recognize any bdc command.
 
I get for instance:
in>background
Error: no such command: background
If the command exists, open the matching component and try it again.

All the other commands (such as go,stop,t,etc.)work well.
 
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

927件の閲覧回数
CrasyCat
Specialist III
Hello
 
What are you trying to achieve here?
What is bdc command expected to do?
 
CrasyCat
0 件の賞賛
返信

927件の閲覧回数
iejiel
Contributor I
Hello CrasyCat,
 
I use mc9rs08ka2 as taget MCU and I want to debbug it using the active background mode commands (read_ status,write_control,etc.) with pemicro usb multilink and cw5.1.
 
I just now received the following explanation that give me the answer:
BDC command can not run in command window. BDC command is a protocol
just for USB HCS08 Multilink communicating with target MCU.
You can type 'help' in command to get all commands that can running in
command window.
So, the commands that you can run in command window and BDC commands
are
very different system.
Generally, Hiwave will send the command you ran in command window to
Multilink and Multilink will translate this command to BDC command and
then send it to target MCU.
Best Regards,
Yong
Technical Support
Freescale Semiconductor
 
 
Thanks,and excuse me,my english is not good I speak spanish.
 
0 件の賞賛
返信