how to get dry battery remain capacity ? - MC1321x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to get dry battery remain capacity ? - MC1321x

1,408 Views
Beijing2008
Contributor I

Dear all:

   I'm using MC1321x with a 3V button battery or 1.5V alkaline battery(dry battery) for supplying power.
   I want to know if HCS08 MCU can get battery voltage? like as lithium battery ,mainly for monitoring the battery state,such as battery low alarm.

 

Look forward to your reply!

Thanks and best regards,
Charly

 

 

Added p/n to subject.


 



Message Edited by NLFSJ on 2008-07-18 09:12 AM
Labels (1)
0 Kudos
Reply
1 Reply

675 Views
bigmac
Specialist III
Hello Charly,
 
Assuming the battery is directly connected to the MCU, there is a low voltage warning (LVW) facility, in addition to the LVD reset.  The state of Vdd relative to the threshold voltage is flagged, and this can be polled.
 
With the low range is selected, the nominal threshold will be 2.1 volts for a falling voltage.  This would seem suitable for a single Lithium cell, or a pair of alkaline cells, to indicate a low battery condition.
 
Regards,
Mac
 
 
 
0 Kudos
Reply