Hi Senthil,
Here is code which i Tested for free running counter configuration .This code toggles (On and OFF) the PORTA for half period of counter value i.e. 128.
code is working fine on PE full chip simulator.
Note: The CPU frequency is in Between 32Mhz to 40Mhz. it depends on your reference frequency so change it in your hardware programmer which is described in my previous comment link.
// prototypes
void main(void);
void COUNTER_Init(void);
void main(void) {
// EnableInterrupts;
/* include your code here */
ICSC2=0x00; // BDIV=0 (Bus Frequency is divided by one)
PTADD =0xFF; // Define Port A as output port
PTAD = 0x00; // Inilise PortA output to Zero
COUNTER_Init(); // Initilise the Counter
for(;;) {
// __RESET_WATCHDOG(); /* feeds the dog */
if (MTIMCNT>128){
PTAD = 0xFF;
}
else {
PTAD = 0x00;
}
}
}
void COUNTER_Init(void) {
MTIMCLK=0x00; // Bus clock (BUSCLK) is selected and Prescaler is zero
MTIMCNT=0x00; // Initilise your counter
MTIMMOD=0x00; // A value of 0x00 puts the MTIM in free-running mode
MTIMSC=0x00; // Start the Timer (TSTP=0 ; Timer start bit) after all above Configuration
}
I hope, this will help you.
Regards
Robin
Hello Pradeep Singh,
Please tell me How to configure this "ICSTRM" internal clock source register ?
the free running counter automatically hardware reset or we need to reset ?
Regrads,
Senthil
Hi Senthil,
There are two ways to reset your Free running counter
1) as soon as you write MTIMCNT=0x00; it will reset the counter and start counting from zero
2) when your Free Running counter overflow i.e. you have 8 bit counter and when MTIMCNT=0xFF;
Automatically in next cycle it will reset to zero , start counting from zero till 0xFF.
can you tell me which hardware you are using to program (Flash) your chip and also your code warrior version than i will tell you how to configure "ICSTRM" register.
One more thing is that above code is working have you tested that?
Regards
Robin
Hi Senthil,
I am using Codewarrior 10.5 so for me The location of the file "9s08sh8.s8p" is as follows
C:\Freescale\CW MCU v10.5\MCU\bin\plugins\support\HC08\gdi\P&E
for you may be it'S in "C:\Program Files\Freescale\CW06 V5.0\prog".
so find out first this file
and at position 10 you will get following line
09BIT_TRIM=004A/004B/01/FFAF/FFAE/001E8480/
The last eight digits 001E8480 has to do with triming. if you convert this value to decimal and multiply with 8 you will get 16Mhz which is Bus frequency and your Counter frequency is double of your Bus frequency cause of the changes in code.
to get 40Mhz Counter frequecy (DCLK) you need 20mhz bus frequency i changed it to 002625A0 ; but as i don't have debugger and programmer so i can't guarantee that's a correct value but u can try.in simulator i am getting bus frequency appx.23Mhz and Counter frequecy appx. 47Mhz which is wrong i know.
you can try it ...i am also trying as soon as i will get solution, will let you know and please tell me the result of above changes in file on controller may be their is some problem in simulator or my interpretation is wrong ...so please let me know the result.
one more, thing in your code add the following lines in place of // ICSTRM=0x50;
ICSTRM = *(unsigned char*)0xFFAE;
Happy programming :smileyhappy:
Regards
Robin
Hello ,
I am using DEMO9S08SH8 development board and Code warrior version 6.3. I wrote a LED blink code but not Not working. Please any one can upload LED Blink working code.
My LED Blink code is,
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
#include "MC9S08SH8.h"
void main()
{
PTCDD_PTCDD0 = 1;
PTCDD_PTCDD1 = 1;
for(;;)
{
PTCD_PTCD0 = 1;
PTCD_PTCD1 = 1;
        for(i=0;i<50000;i++);
       
PTCD_PTCD0 = 0;
PTCD_PTCD1 = 0;
for(i=0;i<50000;i++);
}
}
Hi Senthil,
Here is correction in your LED Code ,it's working fine
int i=0;
PTCDD =0xFF; // Define Port C as output port
PTCD = 0x00; // Inilise Port C output to Zero
for(;;)
{
for(i=0;i<50000;i++){
PTCD_PTCD0 = 1;
PTCD_PTCD1 = 1;
}
for(i=0;i<50000;i++)
{
PTCD_PTCD0 = 0;
PTCD_PTCD1 = 0;
}
}
Happy Progaming :smileyhappy:
Regards
Robin
Hi Senthil,
the problem is in "Int i" definition ,
cause "int i" varibale Range of decimal value is "-32768..+32767" as soon as you will change it to "unsigned int i " it's become 0..65535;
in for loop you have defined it I=50,000 which is greater than 32000
so either you can defined it "unsigned Int i" and try the code has to work or you can change the value in for loop instant of 50000 to 25000 .
The code must work.
Let me know after changes the code is working or not.
Regards
Robin
Hello Robin,
Hi LED code working fine . thank you.
I am using DEMO9S08SH8 development board and Code warrior version 6.3.
I have few questions,
1. I got example code for clock initialization at bus frequency 20 Mhz but How can i ensure that.
that code is,
ICSC1_CLKS = 0;
ICSC1_IREFS = 1;
ICSC1_RDIV = 0;
ICSC2_BDIV = 0;
ICSTRM = 0x58;
2. I have configured free running timer at bus frequency 20 Mhz and pres caller divider 256.
How to find out timing of each count ( I want know the counter incrementing time period)
freerunning code is,
Please any one help me.
MTIMCLK=0x08
MTIMCNT=0x00
MTIMMOD=0x00
MTIMSC=0x00;
Regards
Senthil
Hello Robin,
With your great help, we were able to finally reach to the below working code:
void main(void)
{
UINT16 localCntr_25ms = 0;
UINT8 portToggle = 0;
SOPT1 = 0x03; // disbale watchdog
ICSC1_CLKS = 0; // TODO senthil
ICSC1_IREFS = 1;
ICSC1_RDIV = 0;
ICSC2_BDIV = 3; // 32MHz/8 => 4MHz, fsys is 4MHz and fbus = fsys/2 => 2MHz.
//ICSTRM = 0x96;
MTIMCLK=0x08; // Bus clock (BUSCLK) is selected and Prescaler is 256
MTIMCNT=0x00; // Initilise your counter
MTIMMOD=0x00; // A value of 0x00 puts the MTIM in free-running mode
MTIMSC=0x00; // Start the Timer (TSTP=0 ; Timer start bit) after all above Configuration
PTBDD_PTBDD7 = 1; // Define Port C as output port
SOPT1 = 0x03; // disbale watchdog
for(;;)
{
// with above settings, the MTIMCNT changes every 128us.
if (MTIMCNT > 200)
{
// 25.6ms
localCntr_25ms++;
// MTIMCNT = 0;
MTIMSC_TRST=1;
}
if (localCntr_25ms > 40)
{
// approx. 1000ms
portToggle++;
PTBD_PTBD7 = (portToggle & 0x01);
localCntr_25ms = 0;
}
}
}
Regards,
Senthil,
Hello,
I am working DEMO9S08SH8 development board with CW V6.3.
My GPIO interrupt is not working. my code is ,
void main()
{
PTBSC_PTBIE = 0; // Disable interrupt
PTBPS_PTBPS0 = 1; // PortB, bit-0 is enabled for interrupt
PTBSC_PTBMOD = 0; // edges only
PTBES_PTBES0 = 0; // interrupt on falling edge
PTBSC_PTBACK = 1; // acknowledge flag
PTBSC_PTBIE = 1; // enable interrupt
| PTBDD_PTBDD0 = 0; | 
EnableInterrupts;
for(;;)
{
;
}
}
interrupt 21 void PORTB_ISR(void)
{
PTBSC_PTBACK = 1; // acknowledge flag
}
Please any one help me
Hello Senthil,
Here is Timer configuration for Free running counter for S08RNA16/8/4 CONTROLLER .
FTM0_CNT = 0x0000; // The FTM Counter is Free Running Counter by Defining MODH:L=0x0000 or MODH:L=0xFFFF;
FTM0_MOD = 0xFFFF;
FTM0_SC = 0x0F; //CPWMS=0; Counter Mode;System Clock (Deafult) 16 Mhz, FEI mode Default, Prescaler Factor 1:128
Hope it will help you.
Regards
Robin
Hello Senthil,
Here is System Frequency configuration for S08RNA16/8/4 CONTROLLER .
ICS_C1 = 0x04; // internal reference clock (31250to39250Hz) to FLL (512) and FLL is generating 16000-20000 Khz ; Ref. Freqeuncy is set at 31250-39250 Hz * 512 = Appx.16-20 Mhz
ICS_C2 = 0x00; // BDIV = 00, Freq is now 16-20Mhz
BDIV in Default case is ICS_C2=0x02 so the system frequency is in between 8 to 10 Mhz , but you can change the value of BDIV in ICS_C2=0x00 register as i changed above to zero, prescaler 1:1, it means that Your CPU frequency is now in between 16 to 20 Mhz depend on your Reference frequency multiplied by FLL (512).
But this is valid only for MC9S08RNA 16/8/4 type of controller Archt. In your case it may be different. can you tell me which controller you are using?
So i can check and tell you at wht freq. ur CPU is operting.
Regards
Robin