demo9s08QG8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

demo9s08QG8

Jump to solution
1,556 Views
bourineauthierr
Contributor I

Bonjour

Hi

I  try to program a other CPU (s08ctj for example )   with the developpment kit  Demo9s08QG8 but

codeWarrior don't want to do it.

The error message is : no device available

I thought that was possible with l'USB/BDM integrated on the board

 

please excuse my bad english

thank for your help

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,349 Views
david_diaz
NXP Employee
NXP Employee

Bonjour,

Unfortunately, it is not possible to program a MCU with any DEMO board.

You can program a S08QE8 MCU in a DEMOQE Board for example. But you will never be able to program a S08SH in a DEMOQE.

Bonne journée.

View solution in original post

0 Kudos
Reply
3 Replies
1,349 Views
tonyp
Senior Contributor II

Maybe you want to get yourself a very-very low cost USBDM-compatible board, or even build it yourself (all you need is available.)  There are several versions, so you need to read a bit about them all before you decide which one best suits your needs and pocket.

Start here:

USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.

1,349 Views
bourineauthierr
Contributor I

merci à vous  pour ces renseignements.

0 Kudos
Reply
1,350 Views
david_diaz
NXP Employee
NXP Employee

Bonjour,

Unfortunately, it is not possible to program a MCU with any DEMO board.

You can program a S08QE8 MCU in a DEMOQE Board for example. But you will never be able to program a S08SH in a DEMOQE.

Bonne journée.

0 Kudos
Reply