I use a S08PT60 with code warrior 10.6 and multilink pemicro debug
I use the ADC converter configured without interrupt (ADC_SC1 = 0b00000000;)
When the coco bit is set, i restart the conversion eith other channel :
if (ADC_SC1_COCO)
{
switch (ADC_SC1 & 0x1F)
{
case 0:
First = ADC_RL;
ADC_SC1 = 1;
break;
case 1:
Second = ADC_RL;
ADC_SC1 = 0;
break;
}
When with cw, I suspend the excexution, the ADC crashes and the coco bit remain low.
When crash the ADC register value is the follow
ADC_SC1 0x01 0x0010
ADC_SC2 0x08 0x0011
ADC_SC3 0x00 0x0012
ADC_SC4 0x00 0x0013
ADC_RH 0x00 0x0014
ADC_RL 0x39 0x0015
ADC_CVH 0x00 0x0016
ADC_CVL 0x00 0x0017
ADC_APCTL1 0x03 0x30ac
ADC_APCTL2 0xf0 0x30ad
I have this problem only if break, without break all goes !
I would like to understand why, and fix this annoying problem
Thanks
Stefano