a pager application with 1321xNSK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

a pager application with 1321xNSK

1,488 次查看
crafter
Contributor I
Hi Everybody,

I need assist on my zigbee project  "building a cluster tree messaging network". I thoght end devices will work as a pager. but here is the point should the SARD boards of 1321xNSK be an end device(reduced function device.) and should NCB be a Pan coordinator? or I should find any other product for end devices and set SARD boards for full function device. I m stuck at the beginning. What components do I have to use in this project. and what sources do you suggest me to look.   help of you guys will assist me to go deeper in zigbee world. thanks a lot.

serhat  
标签 (1)
0 项奖励
回复
1 回复

596 次查看
NLFSJ
Contributor III
Hi,
 
Although I may not be able to reply to all your questions, the following information may be of assistance to you:
 
All of Freescale's development boards are programmable and capable of running as an end device (reduced function device) and a coordinator (full function device). 
 
The issue right now is that the ZigBee Stack (BeeStack) will not be released until February.  You can download the BeeKit from the Freescale website and use the 802.15.4 to setup a network
 
Regards,
Nina
0 项奖励
回复