Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Who Tell me the different  between MC908QL4MDW1 and MC908QL4MDW2????? Urgent

2,279件の閲覧回数
harlenChen
Contributor I
We use the MC908QL4MDW.. But the logo on IC is MC908QL4MDW1? And sometimes, the logo is MC908QL4MDW2?  I want to konw the different??? I can not get the information about the '1' or '2' from the datasheet.
thx
Harlen
ラベル(1)
0 件の賞賛
返信
1 返信

938件の閲覧回数
RockyRoad
Contributor III
Harlan -
 
There was a problem with a mask set that the internal clock would not trim to the 25.6 MHz option. These parts are marked with the '1'.  Parts that will trim correctly at 25.6 MHz are marked with '2'.
 
If you are using an external crystal or if you are using the internal at 4, 8, or 12.8 MHz, then this won't make a difference.
 
- Rocky
0 件の賞賛
返信