Whether BKGD signal pin On S08 and S12 series  MCU  need to add pull resistance?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Whether BKGD signal pin On S08 and S12 series  MCU  need to add pull resistance?

1,388 Views
jinhuiwu
Contributor II

Whether BKGD signal pin On S08 and S12 series  MCU  need to add pull resistance?

Labels (1)
0 Kudos
Reply
3 Replies

1,203 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Jinhui

In the S08 case there is not necessary a pull up resistor on the BKGD pin, regarding to the S12 I believe also is not necessary but I am not expert on S12, you can ask on the S12 community

Regards

Vicente Gomez

0 Kudos
Reply

1,203 Views
jinhuiwu
Contributor II

I see!Thanks  for answer!

By the way.I can't program flash.

After identifying,BKGD pin was pulled low.

What causes the BKGD pins to be pulled low?

0 Kudos
Reply

1,203 Views
vicentegomez
NXP TechSupport
NXP TechSupport

maybe the pin is set as a GPIO, please check if you can the BKGDPE = 1

If a debug system is connected to the 6-pin standard background debug header, it can hold BKGD/MS low during a POR or immediately after issuing a background debug force reset, which forces the MCU to active background mode.

Please also check the signal on the reset pin.

0 Kudos
Reply