I think we had this question before and it was indeed a QT4A (although I can't be 100% sure).
But, I wanted to say that you should not eliminate it based on how many SCI ports it has. It could be using the same SCI for separate RX/TX channels (one RX-only, one TX-only), use one hard and one soft SCI port, or even switch between two devices attached to the same port with some hardware help (eg., while talking to the GSM, ignore the GPS, and vice versa).