What is the input voltage range of ADC on MK64FN1M0VDC12?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the input voltage range of ADC on MK64FN1M0VDC12?

2,076 Views
jhhwang
Contributor I
What is the input voltage range of ADC on MK64FN1M0VDC12?
Labels (1)
0 Kudos
Reply
1 Reply

2,006 Views
nxf63973
NXP Employee
NXP Employee

Hi JiHoo

 

The input voltage of the analog-to-digital converter is specified in the  Kinetis K64F Sub-Family DataSheet. It's possible to find  this characteristic in chapter 3.6.1 on the table 30 of this document, as it is shown below.

pastedImage_2.png

The Input voltage (VADIN) accepts values between the ADC reference voltage low and high (VREFL and VREFH). This reference voltages depend on the value of the ground voltage (VSSA) and the supply voltage (VDDA).

 

Then, the  ADC input voltage range is 0 ±100mV  to 3.6V±100mV(depending on the supply voltage).

 

Please let me know if you need any more information.

Jose

0 Kudos
Reply