Wakeup with CAN on 9S08DZ32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wakeup with CAN on 9S08DZ32

876 Views
jamesclem
Contributor I

I am trying to wakeup the micro from stop mode with CAN activity but having no luck.  I have an external interrupt on port B that wakes it up. I set a breakpoint at the line after STOP and the port wakeup hits the BP but the CAN wakeup does nothing. CAN works fine in run mode and I verified that SLPAK is true before STOP. Below is the code to configure the CAN wakeup

 

 

 

   CANCTL0_SLPRQ = 1;

   while (CANCTL1_SLPAK == 0) {};

   CANCTL0_WUPE = 1;

 

   CANRIER_WUPIE = 1;

 

    STOP;

 

 

BP->  wakeup_init();

 

Any advice?

Labels (1)
0 Kudos
Reply
0 Replies