Updater Not Working. You may need to check the site.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updater Not Working. You may need to check the site.

2,203 Views
JimDon
Senior Contributor III
To All,

I have observed check for updates not working.
I have submitted a service request, and tech support is seeing the problem as well.
Not sure if this is affecting all installations or not, but just to be sure you
should go here and check for updates.

Labels (1)
0 Kudos
Reply
4 Replies

1,188 Views
fabio
Contributor IV
Hi Jim,

I am also having some trouble with the updater. I have CW 6.0 and CW 6.1 and they both can't update succesfully. When I run the updater tool, it connects to FS website and returns a message telling me that no updates are available.

Best regards
0 Kudos
Reply

1,188 Views
JimDon
Senior Contributor III
Yup, that's the one.
As I said, you can download them, but the system was meant to use the updater, so there are many small ones instead of a few big ones.
Kinda a pain, not to mention you think there are none, since updater said there were none.
I wish you would do a service request, so they know the extent of the problem.


0 Kudos
Reply

1,188 Views
fabio
Contributor IV
I agree, I'll that right now.

Best regards,
0 Kudos
Reply

1,188 Views
fabio
Contributor IV
Freescale answer:

Dear Fabio Pereira,

In reply to your Service Request SR 1-425519449:

Thanks for the request and bring the problem to our attention.
I tested it on my side I can see the same problem. There were some changes in Freescale web that result the updater couldn't work. I will report this issue to the right team.
During the days that the problem is not fixed, please download the patch from the links below:
1. CW6.0 patch:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF26AD
2. CW6.1 patch:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0127260061788213CF333D

Best regards,
0 Kudos
Reply