Undesired FLASH protection on MC9S08QB4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Undesired FLASH protection on MC9S08QB4

ソリューションへジャンプ
914件の閲覧回数
benthie
Contributor II

Hey everybody,

 

my current application uses the flash programming routines from AN3942. At some point my program writes data to the flash (0xFFC0 - 0xFFFF). Everything works fine so far, the data is where I want it to be and when I debug the controller, the FOPT register tells me, that the flash is unsecured (FOPT = 0xC2).

 

If I stop my program and debug it again, then the "device is secured"-dialog pops up.

 

Does anybody has an idea, at which point the securing happens?

 

Regards,

Ben

ラベル(1)
0 件の賞賛
返信
1 解決策
814件の閲覧回数
benthie
Contributor II

I found the problem. I erased the NVOPT bits due to a page erase and did not set the SEC00 bit back to 0. Ref.Manual p.55.

Thank you anyway.

Ben

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
815件の閲覧回数
benthie
Contributor II

I found the problem. I erased the NVOPT bits due to a page erase and did not set the SEC00 bit back to 0. Ref.Manual p.55.

Thank you anyway.

Ben

0 件の賞賛
返信