Unable to Enter Debug Mode via Cyclone Rev B If Target is 1.8V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Enter Debug Mode via Cyclone Rev B If Target is 1.8V

Jump to solution
1,473 Views
Designer11
Contributor IV

Hello Everyone,

 

I'm having a really strange issue between the micro 9S08QE32 and Cyclone Pro Rev B. If the micro is running at 3.3V, the Cyclone is able to enter debug mode without any problem. However, when the micro voltage is at 1.8V (which is within the micro specification) the Cyclone refuses  to enter debug mode. I believe the Cyclone will work with 1.6V to  5V.  Is there any setting on the cyclone i can change to make it works ?

 

Environment:  CodeWarrior for MCU version: 10.5

 

Thanks,

Vu

Labels (1)
0 Kudos
Reply
1 Solution
1,292 Views
Designer11
Contributor IV

Hi,

Problem solved. The VDD pin 6 on the programing header needs to connect to the micro power supply so that BKGD and RESET lines have a reference voltage. Somehow my cyclone pro B has a 3.2V presents on pin 6 (problem for another day). But the actual solution is the micro WON"T get into debug/programing mode at 1.8VDC. I even tuned the power supply to 1.85V and still no luck. The datasheet said the micro will operate between 1.8V to 3.6VDC. However, the minimum voltage you need is 1.94VDC. I've wasted two days to find this out. 

Thanks,.

View solution in original post

0 Kudos
Reply
1 Reply
1,293 Views
Designer11
Contributor IV

Hi,

Problem solved. The VDD pin 6 on the programing header needs to connect to the micro power supply so that BKGD and RESET lines have a reference voltage. Somehow my cyclone pro B has a 3.2V presents on pin 6 (problem for another day). But the actual solution is the micro WON"T get into debug/programing mode at 1.8VDC. I even tuned the power supply to 1.85V and still no luck. The datasheet said the micro will operate between 1.8V to 3.6VDC. However, the minimum voltage you need is 1.94VDC. I've wasted two days to find this out. 

Thanks,.

0 Kudos
Reply