USB in-circuit programmer for the MC68HC908JB8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB in-circuit programmer for the MC68HC908JB8

3,377 次查看
DMK
Contributor I
I want to implement a method of in-circuit programming of FLASH memory via the USB for 908JB8 microcontroller (application note AN2398) in my application. Is there a possibility to use the USBICP.sys driver or library ISPdll.dll in my code? If yes, how can I receive the  header files for this software?
Thanks!
标签 (1)
0 项奖励
回复
2 回复数

974 次查看
DMV
Contributor I
AN2398 is incomplete, seems that the WDM used is a third party licensed product valued at 2500EUR (The**con).
 
I am attempting to work around having to use a WDM Kernel driver and to make it cross platform by using http://libusb.sourceforge.net  http://libusb-win32.sourceforge.net and http://www.icsharpcode.net/OpenSource/SD/  see attached.
 
Let me know if you can assist david@dmvdesigns.com
 
 
 
 
 
 
0 项奖励
回复

974 次查看
DMV
Contributor I
Got it working at LAST! Cross platform too!!
 
Seems softec (www.softecmicro.com)
USB to MON08/BDM reference design 
failed to lauch.
 
0 项奖励
回复